Other Parts Discussed in Thread: MOTORWARE, CONTROLSUITE
Hi,
I had previously successfully finished motor identification in lab2. I reinstalled CCS5 and the c2000 compiler on my PC for my DRV8301-69m-kit, and now I encounter this problem when debugging lab2b:
-------
load problem error
encountered a problem loading file
C:\ti\motorware\motorware_1_01_00_12\sw\solutions\instaspin_foc\boards\drv8301kit_revD\f28x\f2806xF\projects\ccs5\proj_lab02b\Release\proj_lab02b.out
Could not open file
------
when exploring that directory I could not find the Release folder nor can I find proj_lab02b.out, even when I had clicked on build. I had installed the c2000 compiler through help->update in CCS5. Any idea as to the cause of this error? Incidentally I encounter this problem except for lab 1 and 2 which I had built before reinstalling CCS5 and compiler.
Help is much appreciated! Thanks
Yue