Other Parts Discussed in Thread: DRV8301, INSTASPINUNIVERSALGUI, MOTORWARE
Hi Chris.
I have drawn the pcb a few week ago using the DRV8301 and TMS320F28069MPZT control boards scheme. But, i have a few problems.
I'm using the low inductance and high speed motor. I'm identifying the motor with using DRV8301 Rev.D kit, TMS320F2869MPZT control board and Instaspin GUI for get the parameters. Motor turns smoothly and torque is very strong. But, i don't get the same performance in motor when i using the same parameters with our board. There are approximately 20% loss of torque. I tried to read parameters using the GUI with our board. But the GUI didn't recognize the board.
Now, I want to ask you a few things.
1- How do I solve this torque problems in our card?
2- How do I communicate with the GUI to our board as DRV8301 Rev.D kit?
Methinks, will solve the problem read the parameters by using the GUI with our board.
Best regards.