This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with 28335 TBSTS.bit.Synci register

Hi everybody,

I have a question about the TBSTS.bit.Synci register.

In the epwm manual it says that this register Reading a 1 on this bit indicates that an external synchronization event has occurred. However, whenever I enable GPIO 32 as a synchronous input, even there is no external synchronization on GPIO32 this register still read a 1 whenever I ran the code. (if I disable GPIO 32 asEPWMxSYNCI  this bit reads an 0 instead)

Is there anybody knows why this happens?

Regards,

Jianyang Liu