Other Parts Discussed in Thread: DRV8412, CONTROLSUITE, DRV8312
I have a DRV8412-C2-KIT Rev G working with the Crosshairs Embedded GUI. DRV8412GUIv9.out has been loaded into the control board, and I'm using the DRV8412GUIv9.exe for graphical control of the motor. It works nicely.
But I need to create a custom GUI which allows me to adjust motor settings automatically: turn the motor on for some period of time in one direction, wait, return to the beginning, wait, and execute for a number of cycles or times.
1) Is there source code available for the Crosshairs GUI? It seems that the company no longer supports this tool. I can find only business information, no technical information about the company or code sources.
2) Is there an interface specification for the GUI to board communication? I can figure it out from the DRV8412 control board source, but I'd rather not have to.
Thank for helping...