HI
In one of the documents found on TI website i found that ADC in F28335 is SEQ and on F28069 is SOC:
I read the technical documents for both but I still Can't make out the difference.Is there any?If then what is it?
Kindly help
Thanks Sneha
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
In one of the documents found on TI website i found that ADC in F28335 is SEQ and on F28069 is SOC:
I read the technical documents for both but I still Can't make out the difference.Is there any?If then what is it?
Kindly help
Thanks Sneha
Hi Sneha,
F28335 is a Delfino device and is very very powerful if compared with F28069 which is a Piccolo Device. The major difference being the computation speed is tremendous in F28335, number of communication buses, number of ADCs and ePwms and more.
On the other hand F28069 has a CLA unit, VCU & USB peripheral (optional)
Regards,
Gautam
Hi Gautam
Sneha
Gautam Iyer said:F28335 is a Delfino device and is very very powerful if compared with F28069 which is a Piccolo Device. The major difference being the computation speed is tremendous in F28335, number of communication buses, number of ADCs and ePwms and more.
I know that .I am particularly asking the difference between ADC's of both and why it has been specifically menetion SEQ based for 28335 and SOC based for 28069.
Thanks
Sneha Thakur said:I am particularly asking the difference between ADC's of both and why it has been specifically menetion SEQ based for 28335 and SOC based for 28069.
Ok...
F28335 has a special sequencer that has a auto-sequencing capability.
This facility is not available in F28069. Read the below data for F28069:
Regards,
Gautam
Sneha Thakur said:I was referring a wrong datasheet for F28069 by mistake..
No problem... Happens!
Goodluck & Regards,
Gautam
Hi Sneha,
The F28335 ADC can be configured for 1 sequence of up to 16 conversions or 2 sequences of up to 8 conversions each. The first sequencer can be triggered by ePWMA or an external pin and the second sequencer can be triggered by ePWMB (the combined sequencer can be triggered by all 3 sources). The S+H window duration can be configured globally to the ADC for all conversions.
The ADC for 'Piccolo' series devices (including F28069) has 16 individual SOCs. Each SOC can be configured for a different trigger source (each of the 3 CPU timers, ePWM A or B from each of the ePWM modules, or an external pin) and each can be configured for a different S+H duration. The 16 SOCs can be combined into any number of individual sequences by using the same trigger source for multiple SOCs.
In most cases, the SOC based sequencer is more flexible and powerful, but there are some sampling schemes that work better on the F28335 style sequencer.
Hi,
For the same float point multiplication, for example 1.414*1.732, how many cycles 28335 needs and how many 28069 (with or without CLA)?
Because they both support float point naturally.
Thanks.
Thanks Gautam.
If they have the same clock speed, the time consumed for that calculation should be same?
Sorry I didn't pay attention of the title of this post.