This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir
I'm using the project GUI_project_InstaSPIN_BLDC of DRV830x-HC-C2-KIT_v104.
My motor is BLDC.
The MaxSpeed is 1000RPM. If I want more speed, like 2000RPM, how do I need to do?
Cause I modify the Gui.Ref to 1.2, the FaultFlag will set to 1, and shut down all kits.
Regards,
Hank