Other Parts Discussed in Thread: CONTROLSUITE
I got with the ControlSuite I have when tried to link the example for the piccolo controlstick:
error: file
"../2806x_BootROM_API_TABLE_Symbols.lib<TMS320x2806x_boot_rom_out___romApi_F
lash2806x_Verify_tmp.obj>" specifies ISA revision "C2800", which is not
compatible with ISA revision "C2700" specified in a previous file or on the
command line
error: file
"C:/ti/controlSUITE/libs/utilities/flash_api/2806x/v100/lib/rts2800_ml.lib<b
oot.obj>" specifies ISA revision "C2800", which is not compatible with ISA
revision "C2700" specified in a previous file or on the command line
So it seems the API lib is with version C2700. Where can I have an update for the version C2800 ?
Thanks,
-T