This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5v0 power supply for F28069 controlSTICK

I'm using f28069 controlSTICK, it works fine with power suppy via USB port. It can also work with 3v3 at external pin 4 and GND (external pin 32). Unfortunately, I only have power source at 5v0, if using 3v3 I must have a converter from 5v0 to 3v3.

I see that external pin 16 is 5v0, but with a comment : 'disabled by default'. Could I use this pin for my project ?

Thanks all,

Tam