Other Parts Discussed in Thread: CONTROLSUITE
Hello,
I am trying to set the AUX clock using the following function, SysCtlAuxClockSet(). Once in the function it hangs on the following,
//Wait for the SYSPLL lock
while(ClkCfgRegs.AUXPLLSTS.bit.LOCKS != 1)
{
// Uncomment to service the watchdog
// ServiceDog();
}
I had this working in bare metal configuration, but once I merged this to our development project that uses SYS/BIOS, this happened. I read somewhere that it has something to do with InitSysCtrl();, but I am not sure. Our program starts by doing initial board setup (including InitSysCtrl();) and then runs the BIOS. Once started, I try to setup the USB, and that is where it gets trapped in that loop.
PS. Using F28377D