Other Parts Discussed in Thread: TMS320F28335
Hi,
We have designed a board using TMS320F28335. The processor got connected using the JTAG emulator (BH-USB2000). before loading the program there is a clean clock out on the XCLOCK pin of the processor. But when i load the program and execute the code; the clock disappears and the program also does not get executed.
I am using 30MHz crystal as the input clock source.
In case any more info.is reqd please ask.