Other Parts Discussed in Thread: MOTORWARE
Hello, Chris,
I am using DRV8312-69M-KIT to test a sensorless system. My encoder is Magnetic Quadrature encoder AS5047D.
Motorware version is 13 and CCS version is 5.5.0.
Now I can run the project 12b and 12c. But there are some problems.
For the project 12b, I can not set a negative speed. If a negative speed the motor will stop. It will rotate normally when a positive speed.
For the project 12c, if rotating the motor clockwise, the system will not make the motor go back to the postion 0. if rotating the motor anti clockwise, the position control function works. I think the problem is that the motor can not rotate anti clockwise.
Then I go bakc the project 2a, 2b and others. In project 2a, the speed can be set to a negative value and it will rotate anticlockwise. but in project 2b and others, the motor can not rotate anti clockwise.
How can I check my problem?
Thank you
Fei