Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need hints about ADC with DMA, F28377D

Hi,


Sorry for my asking, but there is no example to follow, and I found nothing by my self-study. I need to know how to use the ADC's interrupt to trigger the DMA.

Some of my codes:

------------

    // Map ISR functions.
    EALLOW;
    PieVectTable.ADCA1_INT = &adca1_isr; //function for ADCA interrupt 1
   EDIS;

   // enable PIE interrupt
    PieCtrlRegs.PIEIER1.bit.INTx1 = 1;      // interrupt of ADC
    // Enable global Interrupts and higher priority real-time debug events:
    IER |= M_INT1;             // Enable group 1 interrupts
    EINT;                      // Enable Global interrupt INTM
    ERTM;                      // Enable Global real-time interrupt DBGM

...

    AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 0;         // end of SOC0 will set INT1 flag

....

interrupt void adca1_isr(void)
{

...

}

-------------------

Above is the configure of ADC, and each time the ADC interrupt can work very well.

------------------

void DMA_configure(void)
{
    EALLOW;
    CpuSysRegs.SECMSEL.bit.VBUS32_1 = 1;
    EDIS;

    /*for (i=0; i < RESULTS_BUFFER_SIZE; i++) {

        DMABuf1[i] = AdcaResultRegs.ADCRESULT0; // Initialize Buffer;
    }
    */
    DMAInitialize();
/*
    DmaRegs.DMACTRL.bit.HARDRESET = 1;  // Perform a hard reset on DMA
    __asm (" nop");               // one NOP required after HARDRESET
    DmaRegs.DEBUGCTRL.bit.FREE = 1;     // Allow DMA to run free on emulation suspend
 */
    // Initialize the DMA
    // DMA Source is buffer 2, destination is buffer 1
    DMA1Source = &AdcaResultRegs.ADCRESULT0;
    DMA1Dest = &DMABuf1[0]; //DMA destination;

    DMACH1AddrConfig(DMA1Dest,DMA1Source);
/*
     // Set up SOURCE address:
    DmaRegs.CH1.SRC_BEG_ADDR_SHADOW = (Uint32)&AdcMirror.ADCRESULT0;    // Point to beginning of source buffer
    DmaRegs.CH1.SRC_ADDR_SHADOW =     (Uint32)&AdcMirror.ADCRESULT0;
    // Set up DESTINATION address:
    DmaRegs.CH1.DST_BEG_ADDR_SHADOW = (Uint32)&DMABuf1[0][0];       // Point to beginning of destination buffer
    DmaRegs.CH1.DST_ADDR_SHADOW =     (Uint32)&DMABuf1[0][0];
 */
    // Set up to use 16-bit data size
    // Pointers are based on 16-bit words
    // Increment by 1 (16 16-bit words)
    DMACH1BurstConfig(ONE_WORD_BURST,SOURCE_NO_ADDRESS_CHANGE,DESTINATION_INCREMENT_ONE_ADDRESS);                                  // BURST size = 1 | Source step size = 0 | Dest step size += 1
/*
    // Set up BURST registers:
    DmaRegs.CH1.BURST_SIZE.all = NumberOfChan-1;//Number of words(X-1)x-ferred in a burst
    DmaRegs.CH1.SRC_BURST_STEP = 1;  // Increment source addr between each word x-ferred
    DmaRegs.CH1.DST_BURST_STEP = NumberOfSamples; // Increment dest addr between each word x-ferred
 */
    DMACH1TransferConfig(TRANSFER_SIZE_0x800,TRANSFER_STEP_SOURCE_NO_CHANGE,TRANSFER_STEP_DEST_INCREMENT_ONE_ADDRESS);            // Transfer size = 0x1000 | Source step size = 0 | Dest step size += 1
/*
    // Set up TRANSFER registers:
    DmaRegs.CH1.TRANSFER_SIZE = NumberOfSamples-1;//(NumberOfSamples-1);                  // Number of bursts per transfer, DMA interrupt will occur after completed transfer
    DmaRegs.CH1.SRC_TRANSFER_STEP = 1;// TRANSFER_STEP is ignored when WRAP occurs
    DmaRegs.CH1.DST_TRANSFER_STEP = 0;// TRANSFER_STEP is ignored when WRAP occurs
 */
    DMACH1WrapConfig(0xFFFF,0,0xFFFF,0);
/*
    // Set up WRAP registers: wrap on 4 reads of ADC
    DmaRegs.CH1.SRC_WRAP_SIZE = NumberOfChan-1;             // Wrap source address after N bursts
    DmaRegs.CH1.SRC_WRAP_STEP = 0;              // Step for source wrap
    DmaRegs.CH1.DST_WRAP_SIZE = 0;              // Wrap destination address after N bursts
    DmaRegs.CH1.DST_WRAP_STEP = 1;              // Step for destination wrap
 */
    PieVectTable.DMA_CH1_INT = &local_DMACH1_ISR;
    // DMA_ADCAINT1 as peripheral interrupt source
    DMACH1ModeConfig(DMA_ADCAINT1,PERINT_ENABLE,ONESHOT_DISABLE,CONT_ENABLE,SYNC_ENABLE,SYNC_SRC,OVEFLOW_ENABLE,SIXTEEN_BIT,CHINT_END,CHINT_ENABLE);
/*
        Select Value (8-bit) DMA ChTrigger Source
        0 No Peripheral
        1 ADCA.1
        2 ADCA.2
        3 ADCA.3
        4 ADCA.4
        5 ADCAEVT
        6 ADCB.1
        7 ADCB.2
        8 ADCB.3
        9 ADCB.4
        10 ADCBEVT
        11 ADCC.1
        12 ADCC.2
        13 ADCC.3
        14 ADCC.4
        15 ADCCEVT
        16 ADCD.1
        17 ADCD.2
        18 ADCD.3
        19 ADCD.4
        20 ADCDEVT

    DmaRegs.CH1.MODE.bit.PERINTSEL = DMA_SEQ1INT;     // Passed DMA channel as peripheral interrupt source
    DmaRegs.CH1.MODE.bit.PERINTE = PERINT_ENABLE;   // Peripheral interrupt enable
    DmaRegs.CH1.MODE.bit.ONESHOT = ONESHOT_DISABLE; // Oneshot disable
    DmaRegs.CH1.MODE.bit.CONTINUOUS = CONT_ENABLE;  // Continous enable
    DmaRegs.CH1.MODE.bit.SYNCE = SYNC_ENABLE;      // Peripheral sync enable/disable
    DmaRegs.CH1.MODE.bit.SYNCSEL = SYNC_SRC;      //Sync effects source or destination
    DmaRegs.CH1.MODE.bit.OVRINTE = OVEFLOW_ENABLE;//Enable/disable the overflow interrupt
    DmaRegs.CH1.MODE.bit.DATASIZE = SIXTEEN_BIT;        // 16-bit/32-bit data size transfers
    DmaRegs.CH1.MODE.bit.CHINTMODE = CHINT_END;     // Generate interrupt to CPU at end of transfer
    DmaRegs.CH1.MODE.bit.CHINTE = CHINT_ENABLE;         // Channel Interrupt to CPU enable

    // Clear any spurious flags:
    DmaRegs.CH1.CONTROL.bit.PERINTCLR = 1;          // Clear any spurious interrupt flags
    DmaRegs.CH1.CONTROL.bit.SYNCCLR = 1;            // Clear any spurious sync flags
    DmaRegs.CH1.CONTROL.bit.ERRCLR = 1;             // Clear any spurious sync error flags

    // Enable DMA INTn in the PIE: Group 7 __interrupt 1-6
    PieCtrlRegs.PIEIER7.bit.INTx1 = 1;  //DMACH1 interrupt

    // Enable CPU INT7 interrupts are enabled
    IER |= M_INT7;  // interrupt group 7
 */

   StartDMACH1();
/*
    EALLOW;
    DmaRegs.CH1.CONTROL.bit.RUN = 1;   //   StartDMACH1();
    EINT;
*/
}



__interrupt void local_DMACH1_ISR(void)
{
    DMA_Done = 0x0001;
    EALLOW;
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP7;
    EDIS;
    ESTOP0;
}

----------------

Above is the DMA part. I called the  "DMA_configure()" in "main()" function; each time, when the ADC gets the data, it will trigger interrupt function "adca1_isr()" to save data, but the DMA part never works.

Someone asked a similar question in the community, and the advice he got was to study "sdfm_filter_sync_dma_cpu01.c", which didn't do help to me about my problem.

Thanks so much if anyone can help.