Hello,
I am trying to use the C2Prog utility to flash my code to the 2406 through SCI bootload mode. I grounded the two pins BOOT_EN and SPISIMO as instructed in the TMS320LF240x-A Flash Programming guide and it didn't seem to work. The guide also mentions about pulling low the MP/MC pin to put it in MicroController mode, but the 2406 doesn't have it so I wonder if I need to put it in MC mode.
Anyway, C2Prog did not even seem to make any connection:
*** PLEASE RESET TARGET IN SCI BOOT-LOADER MODE ***
Pinging target... no response!
I checked the operating frequency out of the chip to be 40MHz (10MHz x 4PLL), as required by C2Prog.
I know it is an old chip, but please let me know if anyone has experience with this situation.
Thanks,
Erik