This example application demonstrates the operation of the Concerto
//! Ethernet controller using the lwIP TCP/IP Stack. DHCP is used to obtain
//! an Ethernet address. If DHCP times out without obtaining an address,
//! AutoIP will be used to obtain a link-local address. The address that is
//! selected will be shown on the UART.
//!
//! Once an address has been obtained, a simple web server can be accessed
//! through the network. The files served are located in the 'fs' directory.
//! Instead of implementing a full file system, the included command-line
//! application 'makefsfile.exe' is used to convert the 'fs' directory to the
//! header file 'lmi-fsdata.h'. This file contains byte arrays for each file
//! and is accessed using the functions in 'lmi_fs.c'. The header file must be
//! re-generated after any changes to files in the 'fs' directory.
//!
//! For more information on 'makefsfile.exe' usage, run 'makefsfile.exe -?'.
//!
//! UART0, connected to the FTDI virtual COM port and running at 115,200,
//! 8-N-1, is used to display messages from this application.
//!
//! For additional details on lwIP, refer to the lwIP web page at:
//! http://savannah.nongnu.org/projects/lwip/
//
This is the procedure for example program please help in detail working and how to execute program and what is the output for above example
Thanks and regards
akhil