Other Parts Discussed in Thread: TMS320F28335
Hi,
I have a problem with running asin table from flash memory.
My uC is TMS320F28335.
The SPRC990 says:
If a table is not included in the boot ROM of the device, then it must be loaded into the
appropriate memory in the linker command file.
In RAM linker cmd I have section:
IQmathTablesRam : > RAML4, PAGE = 1
and _IQasin() works just fine.
But my application needs to work stand-alone.
I would be really grateful if someone could tell me how should FLASH linker cmd file look like, so I can use _IQasin().
Konrad.