Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I have a problem setting up the HRPWM registers of my F28377D controller: I am using the routine prescribed on TI's wiki (see below) but the weirdest thing happens. If I step by step go through the for loop for successively initializing the HRPWM of my ePWM1, ePWM2,... ePWM10 modules then I can ONLY WRITE TO ODD ePWM modules: ePWM1.HRCFNG register will be set properly when ePWM2, ePWM4, ePMW6 will not!
I also tried to set ePWM3.HRCFNG directly and that didn't work either.
I am really puzzled...Is that a bug ?
Thanks in advance for your help,
Regards,
Francois.
Uint16 j;
// ePWM channel register configuration with HRPWM
// ePWMxA / ePWMxB toggle low/high with MEP control on Rising edge
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
for (j=1;j<=NB_IMPEDANCE_BURST_CHANNELS;j++)
{
(*eHRPWM[j]).TBCTL.bit.PRDLD = TB_IMMEDIATE; // set Immediate load
(*eHRPWM[j]).TBPRD = PWM_5MHZ_MODULATION_PERIOD-1; // PWM frequency = 1 / period
(*eHRPWM[j]).CMPA.half.CMPA = PWM_5MHZ_MODULATION_PERIOD / 2; // set duty 50% initially
(*eHRPWM[j]).CMPA.half.CMPAHR = (1 << 8); // initialize HRPWM extension
(*eHRPWM[j]).CMPB.half.CMPB = PWM_5MHZ_MODULATION_PERIOD / 2; // set duty 50% initially
(*eHRPWM[j]).CMPB.all |= (0 << 8); // initialize HRPWM extension
(*eHRPWM[j]).TBPHS.all = 0;
(*eHRPWM[j]).TBCTR = 0;
(*eHRPWM[j]).TBCTL.bit.CTRMODE = TB_COUNT_UP;
(*eHRPWM[j]).TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
(*eHRPWM[j]).TBCTL.bit.HSPCLKDIV = TB_DIV1; // ePWM CLK = SYSCLOCK
(*eHRPWM[j]).TBCTL.bit.CLKDIV = TB_DIV1;
(*eHRPWM[j]).TBCTL.bit.FREE_SOFT = 11;
(*eHRPWM[j]).CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
(*eHRPWM[j]).CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
(*eHRPWM[j]).CMPCTL.bit.SHDWAMODE = CC_SHADOW;
(*eHRPWM[j]).CMPCTL.bit.SHDWBMODE = CC_SHADOW;
(*eHRPWM[j]).AQCTLA.bit.ZRO = AQ_SET; // PWM toggle high/low
(*eHRPWM[j]).AQCTLA.bit.CAU = AQ_CLEAR;
(*eHRPWM[j]).AQCTLB.bit.ZRO = AQ_SET;
(*eHRPWM[j]).AQCTLB.bit.CAU = AQ_CLEAR;
EALLOW;
(*eHRPWM[j]).HRCNFG.all = 0x0;
(*eHRPWM[j]).HRCNFG.bit.EDGMODE = HR_FEP; // MEP control on falling edge
(*eHRPWM[j]).HRCNFG.bit.CTLMODE = HR_CMP;
(*eHRPWM[j]).HRCNFG.bit.HRLOAD = HR_CTR_ZERO;
(*eHRPWM[j]).HRCNFG.bit.EDGMODEB = HR_FEP; // MEP control on falling edge
(*eHRPWM[j]).HRCNFG.bit.CTLMODEB = HR_CMP;
(*eHRPWM[j]).HRCNFG.bit.HRLOADB = HR_CTR_ZERO;
(*eHRPWM[j]).HRCNFG.bit.AUTOCONV = 1;
(*eHRPWM[j]).HRPCTL.bit.HRPE = 0; // Turn 0 high-resolution period control.
(*eHRPWM[j]).TBCTL.bit.PHSEN = TB_DISABLE;
(*eHRPWM[j]).HRPCTL.bit.TBPHSHRLOADE = 0;
EDIS;
}