Other Parts Discussed in Thread: TMDSHVMTRINSPIN, MOTORWARE
Hey,
I am currently working with the InstaSPIN-FOC/Motion dev kit (TMDSHVMTRINSPIN) and am trying to set the motor spinning at a set frequency. Basically, I want to be able to set the V_q and V_d as constants and the theta (rotor position) as a constant ramp function (or sawtooth if it rolls over to 0deg from 359) in the Inverse Park Transform section of the Block Diagram. This should set the T_a/b/c output to the motor at a set frequency depending on the slope of the theta ramp function.