Other Parts Discussed in Thread: ENERGIA
can lcd sceens like the 20x4 sceens be run on the c2000.
I am asking this as I am confused if you can or not as I see there is a library for them in energia.
also how many interrupt pin on the c2000
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ENERGIA
can lcd sceens like the 20x4 sceens be run on the c2000.
I am asking this as I am confused if you can or not as I see there is a library for them in energia.
also how many interrupt pin on the c2000
Hi Daniel,
daniel lyall said:can lcd sceens like the 20x4 sceens be run on the c2000.
There are no libraries for LCD parallel interface and there seems no work done on the same by any community member. Serial-LCD can be interfaced easily, be it 16x2, 20x4 etc...
daniel lyall said:also how many interrupt pin on the c2000
If you're inquiring about external interrupts - F28027 controller in C2000 launchpad, there are 3.
Regards,
Gautam
is there libraries some where for Serial LCD
the project its for only needs a 20 x 4 lcd
daniel lyall said:is there libraries some where for Serial LCD
You don't need any specific library for serial lcd, you can use the same SCI/SPI peripheral library.
Regards,
Gautam