Other Parts Discussed in Thread: TMS320F28069
Dear all,
Currently i am doing single phase solar grid inverter using TMS320F28069 for client .They are given task list of inverter PROJECT.
One of task is to generate single phase grid tie PLL output.
I used PLL with notch filter library file with sine look up table instead of ADC measured sin value.
But i did not get proper PLL output theta value (Ramp output or saw tooth wave form).
I attached the main source code for your examonation
Please give any valid suggestion to finish PLL task within stipulated time.
I am simulating the InvSine value using graph tool in CCS studio.
#include "F2806x_Device.h"
#include "Solar_IQ.h"
#define table_size 1024 //size of table=1024
#define GRID_FREQ 60
#define PI 3.141592653589
#define ISR_FREQUENCY 50000.0
#define B0_LPF (166.7618719)
#define B1_LPF (-166.4785831)
#define A1_LPF (-1.0)
SPLL_1ph_IQ spll1;
//SPLL_1ph_IQ_NOTCH_COEFF spll_notch_coef1;
// Prototype statements for functions found within this file.
__interrupt void cpu_timer0_isr(void);
extern void InitSysCtrl(void);
extern void InitPieVectTable(void);
extern void InitPieCtrl(void);
float c2, c1;
float sin_table[108]={0,0.1736,0.3420,0.5,0.6427,0.7660,0.8660,0.9396,0.9848,1,
0.9848,0.9396,0.8660,0.7660,0.6427,0.5,0.3420,0.1736,0,-0.1736,-0.3420,
-0.5,-0.6427,-0.7660,-0.8660,-0.9396,-0.9848,-1,-0.9848,-0.9396,-0.8660,
-0.7660,-0.6427,-0.5,-0.3420,-0.1736,0,0.1736,0.3420,0.5,0.6427,0.7660,0.8660,0.9396,0.9848,1,
0.9848,0.9396,0.8660,0.7660,0.6427,0.5,0.3420,0.1736,0,-0.1736,-0.3420,
-0.5,-0.6427,-0.7660,-0.8660,-0.9396,-0.9848,-1,-0.9848,-0.9396,-0.8660,
-0.7660,-0.6427,-0.5,-0.3420,-0.1736,0,0.1736,0.3420,0.5,0.6427,0.7660,0.8660,0.9396,0.9848,1,
0.9848,0.9396,0.8660,0.7660,0.6427,0.5,0.3420,0.1736,0,-0.1736,-0.3420,
-0.5,-0.6427,-0.7660,-0.8660,-0.9396,-0.9848,-1,-0.9848,-0.9396,-0.8660,
-0.7660,-0.6427,-0.5,-0.3420,-0.1736};
//RAMPGEN_IQ rgen1;
SPLL_1ph_SOGI_IQ spll2;
_iq21 inv_meas_vol_inst;
_iq24 InvSine;
char index = 0;
void main(void)
{
InitSysCtrl();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.TINT0 = &cpu_timer0_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
EALLOW;
GpioCtrlRegs.GPADIR.bit.GPIO31 = 1;
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
EDIS;
InitCpuTimers(); // For this example, only initialize the Cpu Timers
ConfigCpuTimer(&CpuTimer0,90,50);
CpuTimer0Regs.TCR.all = 0x4001;
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;
IER |= M_INT1;
EINT;
ERTM;
GpioDataRegs.GPASET.bit.GPIO31 = 1;
GpioDataRegs.GPBSET.bit.GPIO34 = 1;
// SPLL 1ph Notch Filter Method intialization
SPLL_1ph_IQ_init(GRID_FREQ, _IQ21((float)(1.0/ISR_FREQUENCY)), &spll1);
spll1.lpf_coeff.B0_lf = _IQ21(B0_LPF);
spll1.lpf_coeff.B1_lf = _IQ21(B1_LPF);
spll1.lpf_coeff.A1_lf = _IQ21(A1_LPF);
c1 = 0.1;
c2 = 0.00001;
SPLL_1ph_IQ_notch_coeff_update(((float) (1.0 / ISR_FREQUENCY)),(float) (2 * PI * GRID_FREQ * 2), (float) c2, (float) c1, &spll1);
//SPLL_1ph_IQ_init(GRID_FREQ,_IQ21((float)(1.0/ISR_FREQUENCY)),&spll1);
//SPLL_1ph_IQ_notch_coeff_update(((float)(1.0/ISR_FREQUENCY)),(float)(2*PI*GRID_FREQ*2),(float)0.00001,(float)0.1,&spll1);
// Step 6. IDLE loop. Just sit and loop forever (optional):
for(;;)
{
;
}
}
__interrupt void cpu_timer0_isr(void)
{
CpuTimer0.InterruptCount++;
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1; // Toggle GPIO34 once per 50 MICROseconds
spll1.AC_input=(long)sin_table[index] >> 3;
//spll1.AC_input=(long)inv_meas_vol_inst>>3;
SPLL_1ph_IQ_MACRO(spll1);
InvSine = (long)(spll1.sin)>> 3; // InvSine is in Q24
index++;
if(index > 107)
{
index = 0;
}
// Acknowledge this interrupt to receive more interrupts from group 1
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}