Other Parts Discussed in Thread: TMS320F28335, CONTROLSUITE, MAX232, MAX3221
Hai all,
I am working with TMS320F28335 Peripheral Explorer Board and I have configured the GPIO's 84, 85, 86, 87 to select Boot mode through SCI-A.
I am using c2prog tool to download the code into the flash location.
To down load the code to flash we need Boot Mode code where we configure the SCI-A port driver.How to configure the memory location to Jump the code to Boot Mode memory. Please help in resolving this issue.
Please Provide some Application notes or code examples for Boot Loading through SCI-A.
Thankyou,
Lakshmi.