Hi All,
I am a student from China and new to C2000.
I have a f28069 board and have learned several examples in conrtolsuite. But now I try to create my project without links to the source codes so I create 2 folders named include and source. The include for h files and source for c files.
In the include folder contains DSP28x_Project.h, F2806x_Cla_typedefs.h, F2806x_Device.h, F2806x_Examples.h and so on.
The problem is that I can not call the functions in these header files. And I typedef char int8 in the F2806x_Device.h but there are errors when I try to create a new variable with type uint8.
The Attachment contains the source code.
Sorry for my poor english.
Regards,