Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000-Motor Control and PFC Developer's Kit Inverter Question

Hello,

I have generated a PWM. This PWM appears on PWMA, PWMB, PWMC and PWMD. When I probe through the oscilloscope at the points of PWMA, PWMB, PWMC, PWMD (i.e the points directly connected to the micro-controller), I do observe PWM. But when I probe at the motor terminals connector i.e TB1 and TB2 at u,v or w with respect to ground, I do not see a PWM, instead see a 3.3V DC Line.

Can you please help? Why the PWM signals are not transfering from the inverter stage to the motor terminals?