We have a new board w/ a 2806. I've verified all power and xtal is running. It 'connected' to programmer fine in CCStuido. Before programming first time we ran the 10kHz 'frequency test' but its not outputting a signal on ANY pin we select. Have tried two units w/ the same problem. We're in production on another similar board w/ 28015s and never had an issue. Do I need to do something different w/ the 2806??