Other Parts Discussed in Thread: CONTROLSUITE, INSTASPIN-BLDC, MOTORWARE
I am porting a sensorless BLDC motor controller from a LF2407 CPU to a F28020 CPU. I can't find an example InstaSPIN project that supports the F28020 but I do see a project for a F28030. Comparing the two processors I don't see any show-stopping incompatibilities. Working in CCS 5.5 I am trying to adapt the F28030 project but am running into various build issues.
I would like to know if there is an existing F28020 motor control project I can use, or if not, are there any issues that would prevent me from using the modified F28030 project?
I would prefer not to port the existing LF2407 code due to the incompatibilities with in-line asm and CPU architecture, as well as sorting through implementation/design issues.
Regards,
Nancy Burkholder