I was running CCS3.1 on WindowsXP without any problems. I recently upgraded to windows 7, and CCS3 wasn't supported, so I got CCS4.
Spectrum Digital's ezDSPF2812 is suppose to work with CCS4 since drivers come with the install package. However, I am having trouble connecting to it.
I'm not sure with target to use. There are 5 Spectrum Digital connections to choose from, 4 of which have device selection for ezdspf2812.
"Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator", "Spectrum Digital C2000 XDS510LC Emulator", and "Spectrum Digital XDS510USB Emulator" gives me an error "error initializing emulator" when I try to start the debugger to connect to the board.
"Spectrum Digital XDS510 Parallel Port-PCI Emulator" gives me a driver selection box, for which i choose "sdgo2812ezdsp.xml". But on connection, it asks for a license for that feature. I am using the free version which is suppose to work with xds100 and development boards.
I am lost as to how to connect to the board. Which target to I select? The parallel port is on port 0x378 and IRQ 0x07.