Hi , I have question about HVPSFB kit,
If I do the follow instruction from the User's Guide :
Start CCS and Open a Project
To quickly execute this build, follow the following steps:
1.
Make sure that jumpers J8 and J6 on the base board are populated.
2.
By default, resistor R6 on Piccolo Macro of the controller card and jumper J1 are removed to enable – boot from FLASH. Re-populate these two to run and program RAM or program FLASH. Connect USB connector to the Piccolo controller card for emulation.
------
only If I repopulate the R6 and J1 , I could start CCS emulation right?
Would I be able to use the GUI after I repopulate R6 and J1?
thank you .