This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRPFCKIT current fuse

Referring to the 4 Amps fuse of the controller, we are uncertain whether your Developer's Kit would run our motor.

The details are as follows:

Siemens 3-phase AC permanent magnet motor
Power: 1.41 KW
Voltage: 150 V
Current: 10 A

Would it be possible to create a DC Link converter with a capacitor on our own to solve the problem?