Other Parts Discussed in Thread: DRV8312, INSTASPIN-BLDC, CONTROLSUITE, MOTORWARE
I haven used InstaSpin yet so I havent got a chance to look at the pwm signals coming out. For each half bridge, the TI piccolo sends out two pwm signals - 1) for high side - PWMH and 2) for low side - PWML . Is PWMH always inverted signal of PWML, (assuming zero dead time).. Also the dead time generator inside the TI piccolo, does it move both the pwm signals to create the dead time or just changes PWML ??
I am trying to use a motor controller board that only takes three pwm inputs - one for each half bridge and has its own dead time inbuilt but the piccolo sends out 6 pwm inputs so I am bit confused. I have seen pwm signals on BLDC controller, just wondering if InstaSpin uses some steps where both the PWMH and PWML are ever low (with zero dead time) .
Any pictures/waveforms would be very very useful. thanks!