Other Parts Discussed in Thread: DRV8301
Hello!
I’m using Instaspin-foc on an own board based on the DRV8301-HC-C2-KIT for controlling a PMSM with low inductance. The motor has 6 poles. The motor current doesn’t look like a sine wave. There is a heavy collapse at the peak of the sine. The collapse will be bigger by increasing the speed. I think that’s the reason why I don’t achieve higher speed (I get less than half of the nominal speed, n_n=30krpm). Does the Instaspin-FOC use an algorithm to add the third harmonic? This impact is very harsh and I don’t know how to fix this. I also verify the measuring of the current by sampling the ADC-results and visualizing them in the graph window. For better understanding I attached an image of the phase current (blue) and the voltage between two phases (red).
I hope someone has an explanation for this phenomenon or a guess to improve the current profile.
Thanks a lot!