I'm not sure this is the right place, but it seems to me there is a mistake in the following doc:
TMS320x2833x, 2823x External Interface (XINTF) Reference Guide (Rev. D)
Page 8: "Zone 0 starts at address 0x4000 and is 4K x 16....."
Page 9, Figure 1: Zone 0 is shown to be mapped at 0x4000 to 0x5000 while the size is said to be 8K x 16. This should be 4K x 16, the 8K is still from the 281x family.
Can someone confirm this?
Thanks!