Dear all,
I am using F28069 piccolo DSP. I used TZ2(pin no 55,GPIO16 as TZ2 pin configuration) as CBC configuration. I simply pull up this pin with 1k resistor with 3.3Volt supply. I am using PWM7A and PWM8A for gate pulse.
Now i power up the control card and start the PWM7A and 8A . everything is OK. there is 3.3V on TZ2 pin. but after 15 to 20 mins i measure 0.12V on TZ2 pin, because of this CBC is work and output PWM are disable.
I can't found why this happen. I simply pull the resistor on TZ2 pin.There is no other hardware on this. than also why this pin become low? I also observed when this event occurred at that time ambient temperature is above 55 degree. When temperature is decreased to 40 degree automatic TZ2 signal become 3.3V and PWM are generating.
Any one have idea about this?
Thanks