I was able to get the sd_card_m3 example working on the F28M35 ControlCard. The example demonstrates reading an SD card using the FatFS library. I was disappointed that the example does not demonstrate writes. When I tried to execute a write command the program breaks to FaultISR. Since there was no writes in the example, I am inclined to believe that pins were not configured completely or that TI did not fully port the processor to work with FatFS. The library is very straight forward, only three lines of code were needed to create a new file, as shown at the bottom. Very little information was on the forum about using the SD card reader on the F28M35 ControlCard. My expectation is that the example would be preconfigured for writing and reading -- I would like to get some feedback from others before I start digging deeper. Thanks for the help.
FIL fil; // File object fresult = f_open(&fil, "message.txt", FA_CREATE_ALWAYS | FA_WRITE); f_close(&fil)