Other Parts Discussed in Thread: TMS320F28035
Dear supplier,
Could you provide information about the temperature profile recommended for TMS320F28035
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320F28035
Dear supplier,
Could you provide information about the temperature profile recommended for TMS320F28035
Regards,
Thanks for the information about reflow.
Could you help me with the problem i described in the post TMS320F28035 EEPROM EMULATION
DearSupplier,
I developed a digitally controlled power supply using TMS320F28035.
I'm using the Sector D of the Flash memory to emulate an EEPROM, in order to store calibration data.
We have already done a mass production lote with 1500 units, and the EEPROM emulation works fine.
Now we are producing a new lote of this product and we are facing some problems with EEPROM emulation.
I'm using CCS3v3.
The DSC can be programmed using the On-Chip Flash Programmer. However when the product is under operation and the Flash_Erase function is activated the DSC stops working and stays locked.
After that i can repeat the programming process using the On-Chip Flash Programmer, so it seems that the memory is not permanently damaged or locked. But when the Flash_Erase function is used during run time the same behavior happens.
I checked the memory behavior when the Flash API functions are activated.
The defective devices does not show a pattern, some device present the problem with the Flash Erase function and some others with the Flash Program function.
Replacing the DSP the system works with the same firmware.
The marking on the device is shown below:
TMS320 980
F28035PAGT
G4 A - 6AVJJW
G4
Best Regards
Ricardo