Other Parts Discussed in Thread: MOTORWARE
A combined heads-up / request issue:
In Motorware_13, the EST_getAngle_pu function documentation mentions a return value between _IQ_ 0.0 and 1.0, but when running a reverse direction / negative speed, the actual value is between zero and MINUS_1.
Further a request related to this function: The angle value is from 0-1 in electrical angle, for one pole. Is there also a function that includes the number of poles, and will give a 'mechanical angle' in a range (0-1) for a full motor revolution?
(This is not very hard to implement, but in our situation with engine running in torque mode and low speed possibility of reversing caused by changing external load, it is somewhat tricky - Besides, I think this should be a standard function)
Regards,
Harry Kroonen