Hi, Can I use my XDS100v2 on C2000 launchpad to program external chip?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Can I use my XDS100v2 on C2000 launchpad to program external chip?
Hi Dmitrey,
Dmitrey Salnikov said:Can I use my XDS100v2 on C2000 launchpad to program external chip?
This has been discussed earlier too in the forum and the answer is:
Yes, you can but there are lot of modifications that have to be done to the board. Hence, it is recommended to purchase a XDS100v2 emulator which is very economical.
Regards,
Gautam
Thanks, but what modifications do you mean?
As I understand from launchpad schematic, I need to remove optic isolators and connect some wires to jtag pads.
Does it really all?
Dmitrey Salnikov said:As I understand from launchpad schematic, I need to remove optic isolators and connect some wires to jtag pads.
Does it really all?
Yup, exactly. If you're fine with removing components from a Launchpad then you're through.
Also, here's another similar post that you would like to go through:
http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/261676.aspx
Regards,
Gautam