Other Parts Discussed in Thread: MOTORWARE
Hello,
I am having an issue with motor identification for the DRV8301-69M EVM. I have hooked up a 30V, 40A power supply to the HC board with some extra bypass capacitors. I am running the InstaSPIN_MOTION_F2806xM software and trying to do the motor identification test.
It is calculating the stator resistance and Flux (V/F) properly-at least they are repeatable. But, mid way at 50% through the test, the hardware gets a FAULT or just hangs. I have triggered on the FAULT signal, and captured the current waveform on a single phase, as well as the PVDD signal going to the board and the OCTW signal.
On the first page of the attached file:
1st page is the screen shot of when the software hangs.
Second page is the captured waveforms:
CH1 (Yellow) : FAULT (triggered)
CH2 (Cyan): PVDD
CH3(Magenta): OCTW
CH4(Green) : Phase Current
The current waveform at ~2300 RPM looks quite distorted.
I am not sure what is really triggering the FAULT condition. Also there are times where the software hangs, and the FAULT pin is not asserted!
Regardless of FAULT signal being asserted or not, I have not been able to make it complete the test.
Also, where would I find the user.h file so I can change some of the parameters? Such as PWM frequency.
Any comments will be greatly appreciated.