Other Parts Discussed in Thread: DRV8301
Dear all,
I have an elaborate Simulink model for motor control which was previously developed without the intention of actually implementing it on this controller. However, now I do want to implement this model on the F28069M controlcard (with DRV8301 inverter board). What would be the best approach to doing this? I know there is support for C2000 Microcontrollers in Simulink, but I don't know which blocks I have to insert into the model (which IOs etc) and how to merge it all.
Also, would it be better to write the code in CCS directly?