I am using the Flash_Program() function provided in the flash api to write a 64-bit value to the OTP.
Initially I had a problem that the device is reset every time I attempt to write to OTP. I went through the forum and found that interrupts are serviced in the non-critical time periods of the flash API functions. During this time the flash and OTP remain inaccessible which could cause the device to reset.
So, I am currently disabling all the maskable interrupts like this:
asm(" setc INTM") // DINT
Status = Flash_Program(Flash_ptr, buffer, Length, &FlashStatus);
asm(" clrc INTM") // EINT
But now I get Status = STATUS_FAIL_PROGRAM, which means the OTP is not programmed. When I remove the DINT and EINT I can see that part of the value is written to OTP before being interrupted and reset. I am unable to figure out what could cause this behavior.
Thanks in advance!