Other Parts Discussed in Thread: ADS1203, ADS1209, ADS1274
Hi All,
I'm trying to get some feeling with the buildin SDFM filter. I connected a delta sigma ADC with modulator output to a SDFM input and let it convert continuously resulting in a nice 25MHz datastream. The datafilter is setup with OSR (128-1), SINC3, 32bit date representation and is enabled. Now I read data from the filter data register.
in the datasheet is written: The data filter uses 25 bits to represent signed integer in two's complement format. The maximum
possible resolution gives a 25-bit word (-16,777,216 to +16,777,215). Note that this value is only reached
if the delta-sigma modulator is operated at absolute maximum positive or negative full-scale...
Well, what if I'm using a 8-bit converter and go to an absolute positive input? Is the filter data output then also represented in a 25bit word with a stepsize of 256 steps?
Or how do I have to see this? Could someone help me understand the SDFM module and its resolution? The datasheet is a bit brief.
best regards,
Tjarco