Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 F28027 Simulink UART Demux (4) doesnt work

Hi,

i have a problem with the F28027 im trying to get 4 different signals from the SCI and give it to the ePWM, while it works perfekt with 2 Signals it does nothing with 4

 

Setup:

SCI:

Data uint: 16

lenght: 4

Demux: 4

 

Setup for 2 PWMs

Data: uint 16

length: 2

Demux: 2

 

Its really annoying and i cant see the Problem at all.

I appreciate every help.

 

Thanks.