This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC bus input for TMDSHVMTRINSPIN

Hello!

In the Quick Start Guide qsg_gui_instaspin_motion.pdf, it is said under Hardware Set-up 4. d. HVMTR_r1p1 that it is recommended to use a DC bus input.

1. Is there a special reason for the recommendation?

2. What would happen, when one would connect the AC input first?

Thanks in advance!

  • it is just better practice to use a stable DC power source when doing experiments and testing. AC inputs aren't as reliable and adds another variable when testing the control on a real motor.

    but we use the AC input all the time, especially for demonstration on-site.