Other Parts Discussed in Thread: DRV8301, MOTORWARE, CCSTUDIO
Hi,
I have the DRV8301 Drive and Piccolo F28069MISO ControlCard. After setting the whole thing up, I opened InstaSPIN Motion F2806xM and tried to let it identify my motor. With Automatic ID identification method, the progress would only go as far as 45 or 46% where it abruptly stops, giving an "EST_State_Error" status. I have also went through the whole ordeal with recompiling the user.h file and renaming projects' *.out file as appProgram, and placing them in the appropriate folder, but then InstaSPIN Motion could not even identify the Hardware (the green light appears next to the HV Kit 1.1 instead of the DRV8301...)!
I then tried doing this in InstaSPIN F2806xM Universal, and it shines a green light indicating an 'Identified Motor' if I have the "user.h settings" selected, but my motor does not spin at all, and it gives me "CTRL_State_OffLine" and "EST_State_Idle" statuses the whole time. All my parameters in my "user.h" file do show up correctly in the interface though. If I have the "user.h settings" disabled and attempt running it, the Motor Identification has a red light instead, indicating a failure.
There is one thing that bugs me; the LD2 LED on the ControlCard continues to blink if I open InstaSPIN F2806xM Universal, but this doesn't happen at all if I just use InstaSPIN F2806xM Motion. Does the blinking LED mean an error with the connection or hardware setup? Even in CCS v5, when I try to debug a project, it keeps giving me (Error 151 @ 0x0) with a message about problem with connection. I'm not sure if this is the right place to ask this question, but I would really appreciate any sort of help and guidance!
Thank you
.
Regards,
Yau