This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC S/H at the same time, without using simultaneous sampling

Hello all,

If the following configurations are made:

SOC0 - ADCINA0

SOC2 - ADCINB1


And SOC0 and SOC1 happen at the same time, which of the following events (if any) will happen?

1) ADCINA0 is sampled to S/H-A and ADCINB1 is sampled to S/H-B at the same time. Then, ADCINA0 is converted (because SOC0 has priority), then ADCINB1 is converted.

2) ADCINA0 is sampled to S/H-A and then converted.  Then ADCINB1 is sampled to S/H-B and then converted.

My problem is that in my system, SOC0 and SOC2 may or may not happen at the same time.  If they do happen at the same time, I need them both to sample as quickly as possible.  Unfortunately, I can not use the simultaneous sampling feature since the two will not always happen at the same time. 


Thanks in advance!

Edit:  I am using the Piccolo 28035.