This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Project to build a working appProgram.out

Other Parts Discussed in Thread: MOTORWARE, CCSTUDIO

It would be tremendously helpful if you could provide just one project that produces an appProgram.out that works with InstaSPIN_MOTION_F2806xM.exe GUI to turn the motor like the distributed version of InstaSPIN_MOTION_F2806xM.exe does. We really want to use the F28069 in our product line :-)

  • jim,

    I explained this on the other post, and it probably wasn't clear to you since the QSG for InstaSPIN UNIVERSAL was missing from MotorWare _13.

    The GUI you are trying to run ONLY works with the appProgram.out that comes with it, you can't replace with a MotorWare project.  It is a "frozen demo" that doesn't have all the features or update that we have put into MotorWare since release.

    You need to use the MotorWare proejcts. To instrument the variables in the MotorWare projects - following the Projects & Labs User's Guide - you can use the Expressions tab in CCStudio (and we give you scripts to load to populate all variable settings correctly for each lab) or the UNIVERSALGUI (standalone or inside CCS while you are building and debugging projects).

    jim henderson said:
    We really want to use the F28069 in our product line :-)

    Thanks, I hope we can help you get up and running.