Other Parts Discussed in Thread: DRV8301, BOOSTXL-DRV8301, MOTORWARE, CONTROLSUITE
I have Problems with my SPI-communication. When i am debug my program, what is based on Lab12b, i get the following error.
C28xx: Trouble Writing Memory Block at 0xbac1 on Page 0 of Length 0x1: (Error -1142 @ 0xBAC2) Device blocked debug access because it is currently executing non-debuggable code. Choose 'Rude Retry' to disable polite mode and force the operation. (Emulation package 5.1.507.0)
When i am comment my SPI-function the programm works without any error. The Master is the MCU and the Slave is a FPGA. First i want to read one single Register (1 Byte) from the FPGA with a function.
Here are my SPI functions:
/* Send one byte and get one back */
void HAL_SPI_TransReceive(HAL_Handle handle, uint8_t *transdata, uint8_t *receivedata) //-----
{
HAL_Obj *obj = (HAL_Obj *)handle;
SPI_Obj *spiA = (SPI_Obj *)obj->spiAHandle;
SPI_write(spiA,*transdata);
while(1) //Warten bis Übertragung abgeschlossen
{
if(SPI_getIntFlagStatus(spiA)==SPI_IntFlagStatus_Completed)
{
*receivedata=(uint_least8_t) SPI_read(spiA);
break;
}
}
return;
}
/*read a register*/
void ReadSingleReg(HAL_Handle handle, uint8_t reg_addr, uint8_t *receivedata)
{
HAL_Obj *obj = (HAL_Obj *)handle;
SPI_Obj *spiA = (SPI_Obj *)obj->spiAHandle;
uint_least16_t onlinestatus=0x0000;
reg_addr=((0x80)||(reg_addr));
spiA->SPICTL|=0x02; // Chip Select Setzen
HAL_SPI_TransReceive(handle,®_addr,receivedata);
onlinestatus=(uint_least16_t)*receivedata;
onlinestatus=onlinestatus<<(7);
reg_addr=0x3F;
HAL_SPI_TransReceive(handle,®_addr,receivedata);
onlinestatus=(uint_least16_t)*receivedata;
HAL_SPI_TransReceive(handle,®_addr,receivedata);
spiA->SPICTL&=0xFD; // Chip Select Rücksetzen
return;
}
my SPI configuration is:
void HAL_setupSpiA(HAL_Handle handle)
{
HAL_Obj *obj = (HAL_Obj *)handle;
SPI_reset(obj->spiAHandle);
SPI_setMode(obj->spiAHandle,SPI_Mode_Master);
SPI_setClkPolarity(obj->spiAHandle,SPI_ClkPolarity_OutputRisingEdge_InputFallingEdge);
SPI_setClkPhase(obj->spiAHandle,SPI_ClkPhase_Normal);
SPI_enableTx(obj->spiAHandle);
SPI_enableTxFifoEnh(obj->spiAHandle);
SPI_enableTxFifo(obj->spiAHandle);
SPI_setTxDelay(obj->spiAHandle,0x0018);
SPI_setBaudRate(obj->spiAHandle,(SPI_BaudRate_e)(0x0003));
SPI_setCharLength(obj->spiAHandle,SPI_CharLength_8_Bits);
SPI_setSuspend(obj->spiAHandle,SPI_TxSuspend_free);
SPI_enable(obj->spiAHandle);
return;
}
What is the reason of my failure? I hope somebody could help me.
I am calling the function in the MainISR:
ReadSingleReg(halHandle, version, &SPI_Receivedata);