Other Parts Discussed in Thread: TMS320F28335
Hi all,
I am using CCS 6.0.0.00190 for delfino series( TMS320F28335 ).
I have a problem related to setting break point.
I have multiple files from which i cannot set break point in some of the files.
for example I can set break point in "file1.c" but cannot set break point in "file2.c" .Both are in the same project.
Whenever i try to set break point in "file2.c" i get a message
"C28xx: Trouble Setting Breakpoint with the Action "Remain Halted" at 0x307005: Error 0x00000008/-1066 Error during: Break Point, Cannot set/verify breakpoint at 0x00307005
C28xx: Breakpoint Manager: Retrying with a AET breakpoint
C28xx: Breakpoint Manager: Error enabling this function: DCU_SEL Can not get the ID for the ANA register"
could you please suggest the solution.
Regards,
Keyur