Other Parts Discussed in Thread: DRV8301, BOOSTXL-DRV8301
I'm playing with a new motor and I'm having some issues. To get me started I measured the inductance and the DC resistance using an LCR meter and put in roughly the correct rated flux based on the V/Hz. I then let it do an Rs offline measurement and also ran it up to speed and took down the rated flux value.
The motor is an Axi 2212/12 which is supposed to be 1950KV.
So, the DC resistance of this motor phase-to-phase is about 32mohm. I thought we had to divide that by 2 to get the phase-to-neutral value? So why is InstaSPIN getting a resistance of about 30mohm? Similarly the rated flux is quite far off.
The motor actually seems to run reasonably well, but one other strange thing that I've noticed is that if I run the motor unloaded at a constant medium-high speed (say 10-15krpm) then although the speed seems to be quite stable and the motor appears to be spinning very smoothly the torque and Iq are fluctuating wildly (positive and negative.