Other Parts Discussed in Thread: F28M35H52C
Hello,
I need to interface EQEP and ECAP modules of F28M35H52C controller with both NI simulated EQEP/ECAP signals and with actual sensor signals aswell.
Signal Specs: Two 3.3V sqaure waves with 90 degrees apart. Max frequency: 266Hz. Distance between signal source and controller is arounnd 2 meters.
Concern: Since cable length is 2 meters, my idea is to use buffers and noise filters.
This may affect the transition time of signals and may also cause propagation delay. Is my understanding correct??
And please suggest some design techniques for this interface.
Thanks in advance.
Best Regards,
Govind.