Hi All,
The TMS320F28377(D) has Harvard architecture, which is nice, but I can't find the dual mapped memory and peripheral addresses in the datasheet. I only find the ?data-space-mapped? addresses. In the TMS320F2833x the dual mapped addresses have a 2nd memory address specified for program space (+0x3F0000).
If the program-space mapped registers have a offset (like +0x3F0000) am I able to use these addresses with the CLA? Because CLA i's using 16bit adressing?
Or does the linker handle this? Is it enough to set the "page" to zero or one in the command linker file for determining whether the data is fetched through data or program memory bus?
It's a bit confusing..
Best regards,
Tjarco