Other Parts Discussed in Thread: TMS320F28044, LM317
I need to know what is required for proper power sequencing ofthe TMS320F28044. I am using a TPS70102 regulator to bring up the 1.8V corefirst and then the 3.3V I/O. Appnote SPRAAP6A says to bring up the analogvoltage supplies next. Does this mean I have to have both those supplies (VDDCOREand VDDIO) stable before I can bring up the analog supplies VDDA1.8 and VDDAIO?If so in what order? Is it OK if the 1.8V analog comes up at the same time asthe 1.8V core voltage? Or both analog voltages at the same time? The referencedesigns I've seen don't seem to worry about waiting for the analog supplies tocome up until digital displays are stable.